Skip to main content
Visitor II
March 31, 2025
Question

STM32U3 series wake-up from Stop 3 mode on SMPS current/charge discrepancy

The datasheets for the new STM32U3 MCUs (375/385) list wake-up from stop3 on SMPS in uA (current), whereas for LDO the docs list the same specs in charge (nAs).

Checking the U5 datasheet and the numbers are correctly listed in nAs units. However, the values for U3 are 40-60uA, so if I add 's', it will result in fairly high figures. U5 MCU figures are ~150nAs.

Please confirm that if it's 40-60uAs or 40-60nAs, or something else.

Thanks.

This topic has been closed for replies.

1 reply

KDJEM.1
ST Technical Moderator
April 8, 2025

Hello @ArturK, and welcome to the community,

 

Thank you for bringing this issue to our attention.

The unit in table "Current consumption during wake-up from Stop 3 mode on SMPS" should be "nAs" instead of "µA".

This typo is reported internally.

Internal ticket number: 205032 (This is an internal tracking number and is not accessible or usable by customers).

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.