Skip to main content
Associate
Apr 20, 2026 3:03 PM UTC
Solved

STM32U3: 3V3 tolerant GPIO at 1V8 supply ?

Hi,

 

I am using STM32U385CGU6 with 1.8V supply. My GSM peripheral using the 3.3V Uart port for a dedicated time (2sec) then turn back to 1.8V level of UART.  

Could you offer 3.3V tolerant pin? I am using PA8 to communicate with GSM module.

 

thank you & best regards,

 

feramuz karşil

 

waclawek.jan
waclawek.janBest answer
Super User
Apr 20, 2026 3:46 PM UTC

Look at pin/ball definitions table in Datasheet, that lists all pins together with their input/output structure.

Now look at General operating conditions table, that gives the permissible range of voltages for each type of pin. For TT_xx pins, it's generally up to its VDDIO (which except some PGx pins and USB pins is identical to VDD) supply voltage; for FT_xx pins ("five-volt tolerant"), it's up generally up to VDDIO+3.6V or 5.5V, whichever is less.

PA8 is listed as FT_h, so it should be OK if it is turned to input and 3.3V is applied to it. It won't be able to source 3.3V when VDD is 1.8V, though.

JW

3 replies

mƎALLEm
ST Technical Moderator
Apr 20, 2026 3:37 PM UTC

Hello,

From the datasheet (DS14830 - Rev 3) / Table 27. General operating conditions

mALLEm_3-1776699335371.png

mALLEm_2-1776699293959.png

That depends on what you are using as power supply.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
waclawek.jan
waclawek.janBest answer
Super User
Apr 20, 2026 3:46 PM UTC

Look at pin/ball definitions table in Datasheet, that lists all pins together with their input/output structure.

Now look at General operating conditions table, that gives the permissible range of voltages for each type of pin. For TT_xx pins, it's generally up to its VDDIO (which except some PGx pins and USB pins is identical to VDD) supply voltage; for FT_xx pins ("five-volt tolerant"), it's up generally up to VDDIO+3.6V or 5.5V, whichever is less.

PA8 is listed as FT_h, so it should be OK if it is turned to input and 3.3V is applied to it. It won't be able to source 3.3V when VDD is 1.8V, though.

JW

FERAMUZAuthor
Associate
Apr 20, 2026 4:21 PM UTC

Hi JW,

 

thank you for your feedback.

 

 

best regards,