Skip to main content
Visitor II
Apr 22, 2026 8:13 PM UTC
Solved

STM32U083MCT6TR, How should VDDUSB be handled when USB is not used and VDD = 1.8 V?

I’m designing a board using the STM32U083MCT6TR, and my system supply voltage is VDD = 1.8 V.
The design does not use USB at all.

The datasheet specifies that VDDUSB normally requires 3.0–3.6 V for USB operation, but it’s not fully clear what the correct connection is when USB functionality is not needed.

My question:
What is the recommended way to handle the VDDUSB pin when USB is unused and the MCU is powered at 1.8 V?

Should VDDUSB be tied to VDD (1.8 V)?

Should it be left unconnected?

Or is another configuration required?

If anyone has experience with the STM32U0 series or clarification from ST, I’d appreciate the guidance.

Thanks,

-Tal

Gyessine
GyessineBest answer
ST Technical Moderator
Apr 23, 2026 9:00 AM UTC

Hello @Tal 
Based on AN6020 and AN4879, the usual recommendation is to connect VDDUSB to your main supply rail (VDD = 1.8 V).Do not leave VDDUSB floating .Also its recommended to local decoupling capacitor to ground, just like any other supply pin

BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Gyessine
GyessineBest answer
ST Technical Moderator
Apr 23, 2026 9:00 AM UTC

Hello @Tal 
Based on AN6020 and AN4879, the usual recommendation is to connect VDDUSB to your main supply rail (VDD = 1.8 V).Do not leave VDDUSB floating .Also its recommended to local decoupling capacitor to ground, just like any other supply pin

BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.