STM32U083CCT6 HAL_StatusTypeDef Description Section
I am not sure but if this is a minor issue or should be fixed when working with STM32U083CCT6 MCU and those line is inside stm32u0xx_hal.c file.
Note: I can not add picture or drag it i dont know why.
* @brief Configure the Flash prefetch and the Instruction cache,
* the time base source, NVIC and any required global low level hardware
* by calling the HAL_MspInit() callback function to be optionally defined in user file
* stm32g0xx_hal_msp.c.
In the automatic generated comment lines it state that it was in stm32g0xx_hal_msp.c. If those kind of minor issues should be reported somewhere else , i use that place if i come accross the same situation again.(I am working with stm32u0xx by the way via CubeMX selection and code generation)