hello @gilberto-falker
Can you implement the following code in your project?
If everything is implemented correctly, the STM32 enters stop 2 mode after one second and wakes up from it after another second. The PA5 pin will be set to verify the operation. You can use the USERLED for visual verification.
Cube MX configuration:


int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_LPTIM1_Init();
HAL_NVIC_SetPriority(TIM6_DAC_LPTIM1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(TIM6_DAC_LPTIM1_IRQn);
HAL_LPTIM_TimeOut_Start_IT(&hlptim1, 3999);
HAL_Delay(1000);
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
SystemClock_Config();
while (1)
{
}
}
static void MX_LPTIM1_Init(void)
{
hlptim1.Instance = LPTIM1;
hlptim1.Init.Clock.Source = LPTIM_CLOCKSOURCE_APBCLOCK_LPOSC;
hlptim1.Init.Clock.Prescaler = LPTIM_PRESCALER_DIV16;
hlptim1.Init.Trigger.Source = LPTIM_TRIGSOURCE_0;
hlptim1.Init.Trigger.ActiveEdge = LPTIM_ACTIVEEDGE_RISING;
hlptim1.Init.Trigger.SampleTime = LPTIM_TRIGSAMPLETIME_DIRECTTRANSITION;
hlptim1.Init.Period = 3999;
hlptim1.Init.UpdateMode = LPTIM_UPDATE_IMMEDIATE;
hlptim1.Init.CounterSource = LPTIM_COUNTERSOURCE_INTERNAL;
hlptim1.Init.Input1Source = LPTIM_INPUT1SOURCE_GPIO;
hlptim1.Init.Input2Source = LPTIM_INPUT2SOURCE_GPIO;
hlptim1.Init.RepetitionCounter = 0;
if (HAL_LPTIM_Init(&hlptim1) != HAL_OK)
{
Error_Handler();
}
}
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET);
GPIO_InitStruct.Pin = GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}
void TIM6_DAC_LPTIM1_IRQHandler(void)
{
HAL_LPTIM_IRQHandler(&hlptim1);
}
void HAL_LPTIM_CompareMatchCallback(LPTIM_HandleTypeDef *hlptim)
{
if (hlptim->Instance == LPTIM1)
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
}
}
Hope that helps!
Gyessine
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.