STM32U073 Flash Erase Reports success but does nothing
Hello,
In my application using the STM32U073 series MCU I must erase one of the last pages of flash (actually several of them but for this example I’ll just use one).Page 62, addresses 0x0801f000 - 0x0801f800, and when I call HAL_FLASHEx_Erase I get no errors either from the function return or the pageError parameter that gets written to inside the erase function, both report success.
However when I look at the memory with the memory viewer I see that the first words at that page are still not erased. I moved the erase function out of the many layers of other code and tried to execute it directly in main after the peripherals and initializations have been done, but the outcome was the same. This version of the code is attached, as well as screenshots of the debugger with memory view and the UART terminal for debug output.




int main(void)
{
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
//
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_COMP1_Init();
MX_I2C2_Init();
MX_RTC_Init();
MX_COMP2_Init();
MX_LPUART3_UART_Init();
MX_RNG_Init();
/* USER CODE BEGIN 2 */
//Starts the application RTC OP_timer (DEFAULT -> FAST)
set_default_ARTC_timer();
set_test_led(TESTPIN_LOW);
debug_send_string(dbg_GENERAL, "------ "FW_REV_STR);
//Set the initial pin mainSM_state
set_initial_pinstate();
//set_test_pin1(false);
//southcoFlashInit(main_call_back);
FLASH_EraseInitTypeDef eraseInitStruct ={
.Page = 62,
.NbPages = 1,
.TypeErase = FLASH_TYPEERASE_PAGES,
.Banks = FLASH_BANK_1
};
uint32_t PageError = 0;
uint8_t word_holder[4];
memcpy(word_holder, (void*)0x0801f000, 4);
debug_send_bytes("Controller Header Before Erase: ", word_holder, 4);
HAL_FLASH_Unlock();
HAL_StatusTypeDef status = HAL_FLASHEx_Erase(&eraseInitStruct, &PageError);
//FLASH_PageErase(eraseInitStruct.Page);
HAL_FLASH_Lock();
if(status)
debug_send_string(dbg_GENERAL, "HAL Error");
else
debug_send_string(dbg_GENERAL, "HAL Success");
memcpy(word_holder, &PageError, 4);
debug_send_bytes("Page Error Value: ", word_holder, 4);
memcpy(word_holder, (void*)0x0801f000, 4);
debug_send_bytes("Controller Header After Erase: ", word_holder, 4);
}Not Sure if this is related either but for some reason when I try to connect to this device with theSTM32CubeProgrammer application, the connection always fails unless I first run a debug session from the IDE and then terminate and try to connect from the Programmer. Could there be an issue with the debugger tool that is setting/clearing something in a register to make this happen? I know its not directly an issue with the debugger itself as when I run the code without the debugger I get the same behavior
Any help is greatly appreciated!