Skip to main content
Franzi.Edo
Senior
Jun 30, 2026 10:14 AM UTC
Solved

STM32N657 DK - LTDC layer framebuffer corruption when using AXI SRAM (background OK)

Hi,

I am writing my own RTOS and I do not use CubeMX nor the HAL. I directly program the STM32N657 LTDC registers.

The target is the STM32N6570-DK board with the original 800x480 RGB LCD.

Problem description

The LTDC background color is displayed perfectly.

However, as soon as I enable Layer 1 with a framebuffer located in the internal AXI SRAM, the displayed image becomes corrupted.

The corruption is unusual:

  • the top of the image is correct,
  • below approximately 320 lines, the image progressively becomes shifted,
  • the bottom of the image looks like repeated square blocks shifted horizontally,
  • no FIFO underrun is reported.

The framebuffer contents themselves are correct when read back by the CPU.

LTDC configuration

Framebuffer:

Address : 0x34200000
Format : ARGB8888
Size : 800 x 480
Pitch : 3200 bytes

 

Layer registers:

L1CFBAR  = 0x34200000
L1CFBLR = 0x0C800C83
L1CFBLNR = 480

L1PFCR = 0x00000000 (ARGB8888)
L1CACR = 0x000000FF
L1BFCR = 0x00000607
L1CR = 0x00000001

 

Global registers:

GCR  = 0x00012221
SSCR = 0x00030003
BPCR = 0x000B000B
AWCR = 0x032B01EB
TWCR = 0x033301F3

 

Interrupt status:

ISR  = 0
ISR2 = 0

No FIFO underrun is ever reported.

Memory

The framebuffer is located entirely inside AXI SRAM3-6.

The linker reserves:

0x34200000 - 0x343BFFFF

 

The framebuffer occupies:

0x34200000 - 0x34376FFF

No other object is allocated inside this area.

The MPU marks this region as

  • Normal memory
  • Non-cacheable
  • Non-shareable
  • Read/Write
  • Execute Never

The CPU writes the framebuffer correctly.

The DCache is explicitly cleaned after every framebuffer update.

Interesting observation

 

If I reduce the framebuffer height:

100 lines -> OK
200 lines -> OK
300 lines -> OK
320 lines -> still OK
330 lines -> corruption starts
480 lines -> strong corruption

The corruption therefore depends on the framebuffer height.

 

However, moving the framebuffer to

0x34300000

 

and displaying only 100 lines also works correctly.

Therefore the problem does not appear to be tied to a specific SRAM bank.

 

Things already tested

I have already tested all of the following without any improvement:

  • RGB565 instead of ARGB8888
  • Different framebuffer pitches
  • Different burst length (L1BLCR)
  • Different PLL configuration
  • Different LTDC clock frequencies
  • Different layer window sizes
  • Different framebuffer addresses
  • MPU cacheable / non-cacheable
  • Shareable / non-shareable
  • RISAF configuration
  • RIF configuration
  • Cache clean / barriers
  • Different blending modes
  • Background only (always perfect)

Question

Has anybody already experienced this behaviour on STM32N657?

Is there any additional LTDC register that must be configured on STM32N6 (compared to STM32H7)?

Could this be related to an undocumented limitation of the LTDC fetch engine or AXI SRAM access?

Any suggestion would be greatly appreciated.

Kind regards,

Edo

 

Franzi.Edo
Franzi.EdoBest answer
Senior
Jun 30, 2026 5:57 PM UTC

Dear all,
I found both the root cause and the solution.


My graphics application runs inside an RTOS.

When there are no runnable tasks, the OS executes the WFI instruction and waits for the next interrupt.
During WFI, the clocks of many peripherals and memory blocks are gated to reduce power consumption.
The RCC provides LP (Low-Power) enable bits to keep selected peripherals clocked while the CPU is in WFI.

I correctly enabled the LP bits for all the peripherals required by the LTDC, including the LTDC itself, but I completely overlooked the internal AXISRAM that stores the framebuffer.

As a result, when the CPU entered WFI, the LTDC DMA was still running but was reading from memory whose clock had been gated, which produced the corrupted image.

The solution was simply to enable the LP RCC bits for the AXISRAM banks containing the framebuffer.

I hope this helps anyone facing a similar issue.
Kind regards,

Edo

http://www.ukos.ch

 

1 reply

Franzi.Edo
Franzi.EdoAuthorBest answer
Senior
Jun 30, 2026 5:57 PM UTC

Dear all,
I found both the root cause and the solution.


My graphics application runs inside an RTOS.

When there are no runnable tasks, the OS executes the WFI instruction and waits for the next interrupt.
During WFI, the clocks of many peripherals and memory blocks are gated to reduce power consumption.
The RCC provides LP (Low-Power) enable bits to keep selected peripherals clocked while the CPU is in WFI.

I correctly enabled the LP bits for all the peripherals required by the LTDC, including the LTDC itself, but I completely overlooked the internal AXISRAM that stores the framebuffer.

As a result, when the CPU entered WFI, the LTDC DMA was still running but was reading from memory whose clock had been gated, which produced the corrupted image.

The solution was simply to enable the LP RCC bits for the AXISRAM banks containing the framebuffer.

I hope this helps anyone facing a similar issue.
Kind regards,

Edo

http://www.ukos.ch