Skip to main content
Associate II
September 8, 2025
Question

STM32N6 VENC Hardware Handshake with MJPEG encoding

The VENC peripheral on the N6 boasts a hardware handshake path with the DCMIPP peripheral, potentially allowing full compression of each frame to occur with very little active RAM. From what I can find, the DCMIPP capture starts, then the VENC is told to start encoding, and the application only then receives notifications when a frame is complete. There should be no further interaction. However, I am unable to get this working for MJPEG. The examples for this sort of streaming are all for h264, and the JPEG is thrown to the side as a one-time encoding. I have reasons on this project to use MJPEG encoding, but I cannot get the VENC to perform this handshake with the supplied example code. I have attempted to modify the JPEG Encoding Example that uses the VENC, and have successfully used the VENC for JPEG encoding of a full in-RAM frame, so I know the peripheral can work. Relatedly, the only articles on the handshake algorithm I can find is for the H264 compression.

I'm looking for any working examples of JPEG handshake streaming, or any assistance on getting it working. There seems to be many missing functions in the VENC middleware related to this. All of the JPEG functions are full-frame encoding, no support for double-buffering, nor any mention of streaming. I had to hunt down and dig through H264 examples to even figure out that the JPEG configuration had hidden the "HW" mode. 

4 replies

ST Employee
September 10, 2025

Hello @chornbeck,

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.

Best regards,
Maxime

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Will_Robertson
Associate III
December 23, 2025

Hello @Maxime_MARCHETTO and @chornbeck 

I was wondering if you could share the outcome of this? This is functionality that could be very helpful to us as well.

Will

Associate
January 28, 2026

@Maxime_MARCHETTO I'd also like to register my interest in getting ST to dedicate some support effort for this.  It would be very helpful if the middleware could support hardware handshake MJPEG encoding in a similar fashion to H.264, especially because it seems the hardware itself could accommodate it.

chornbeckAuthor
Associate II
December 23, 2025

@Will_Robertson Sadly, the support I got for this boiled down to "We never got that working, but one of our guys in Europe maybe got further than others?". I was unable to get it working on my end either, and was forced to drop the issue due to priority shifts. If you figure this out, I'd love to know.