Skip to main content
Associate
Jun 26, 2025 7:16 AM UTC
Question

STM32N6 series DCMI module

I am very new to this field !! So last I had posted regarding the interfacing of DCMI and I got relevent doucuments which where not enough for me to understand the DCMI module. So could you please send relevant videos of interfacing DCMI module step by step.

This topic has been closed for replies.

2 replies

KDJEM.1
ST Technical Moderator
Jul 1, 2025 10:19 AM UTC

Hello @nishanth;

 

You can find in AN5020 "Introduction to digital camera interface (DCMI) for STM32 MCUs - Application note" and precisely in DCMI application examples section a step-by-step implementation examples.

Also, I recommend you to look at this video STM32H7 OLT - 55. Peripheral Digital Camera Interface DCMI may help you to understand the DCMI features.

Also, you can check the reference manual section 38 Digital camera interface (DCMI).

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
Associate III
Jul 24, 2025 1:08 PM UTC

Hi, 

Use DCMIPP, for DCMIPP you dont need to enable DMA, DCMIPP is much better, and besides - DMA for DCMI do not work because of bug's, don't forget to add HAL_DCMIPP_MspInit routine, cubeMX do not generate and without CLK, IRQ and pinout you will get errors and DCMIPP will not work, adjust by you hw.

/* USER CODE BEGIN 4 */
void HAL_DCMIPP_MspInit(DCMIPP_HandleTypeDef *hdcmipp) {
	GPIO_InitTypeDef GPIO_InitStruct = { 0 };
	RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = { 0 };
	//if (hdcmi->Instance == DCMIPP) {

	__HAL_RCC_DCMIPP_CLK_ENABLE();
 __HAL_RCC_DCMIPP_FORCE_RESET();
 __HAL_RCC_DCMIPP_RELEASE_RESET();
 HAL_NVIC_SetPriority(DCMIPP_IRQn, 3, 0);
 HAL_NVIC_EnableIRQ(DCMIPP_IRQn);

 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_DCMIPP;
 PeriphClkInitStruct.DcmippClockSelection = RCC_DCMIPPCLKSOURCE_IC17;
 PeriphClkInitStruct.ICSelection[RCC_IC17].ClockSelection = RCC_ICCLKSOURCE_PLL3;
 PeriphClkInitStruct.ICSelection[RCC_IC17].ClockDivider = 4;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK) {
 Error_Handler();
 }

	__HAL_RCC_GPIOF_CLK_ENABLE();
	__HAL_RCC_GPIOA_CLK_ENABLE();
	__HAL_RCC_GPIOG_CLK_ENABLE();
	__HAL_RCC_GPIOB_CLK_ENABLE();
	__HAL_RCC_GPION_CLK_ENABLE();
	/**DCMI GPIO Configuration
	 PF1 ------> DCMI_D7
	 PA1 ------> DCMI_D0
	 PG3 ------> DCMI_HSYNC
	 PG15 ------> DCMI_D4
	 PA10 ------> DCMI_D1
	 PG1 ------> DCMI_PIXCLK
	 PG10 ------> DCMI_D2
	 PG2 ------> DCMI_D6
	 PB4(NJTRST) ------> DCMI_VSYNC
	 PN9 ------> DCMI_D5
	 PA4 ------> DCMI_D3
	 */

	GPIO_InitStruct.Pin = GPIO_PIN_1;
	GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
	GPIO_InitStruct.Alternate = GPIO_AF9_DCMIPP;
	HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);

	GPIO_InitStruct.Pin = GPIO_PIN_1 | GPIO_PIN_10 | GPIO_PIN_4;
	GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
	GPIO_InitStruct.Alternate = GPIO_AF9_DCMIPP;
	HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

	GPIO_InitStruct.Pin = GPIO_PIN_3 | GPIO_PIN_15 | GPIO_PIN_1 | GPIO_PIN_10 | GPIO_PIN_2;
	GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
	GPIO_InitStruct.Alternate = GPIO_AF9_DCMIPP;
	HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);

	GPIO_InitStruct.Pin = GPIO_PIN_4;
	GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
	GPIO_InitStruct.Alternate = GPIO_AF9_DCMIPP;
	HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

	GPIO_InitStruct.Pin = GPIO_PIN_9;
	GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
	GPIO_InitStruct.Alternate = GPIO_AF10_DCMIPP;
	HAL_GPIO_Init(GPION, &GPIO_InitStruct);
}