Skip to main content
matt-crc
Senior III
Feb 26, 2026 5:03 PM UTC
Question

STM32N6: In HSE Bypass, can PH1 pin be configured as Input Output ?

 

Split from original question 

Can you check your documentation ?  According to RM086 - Reference Manual for STM32N657, all PH GPIOs can be set as input/output (contradicting your previous post). 

  • Default State: When a crystal is used for the HSE (PH0/PH1), PH1 is dedicated to the oscillator output and cannot be used as a general-purpose I/O (GPIO).
  • Bypass Mode: When you configure the RCC (Reset and Clock Control) to "HSE Bypass," an external clock signal is fed directly into PH0 (OSC_IN), freeing up the PH1 pin to act as a standard GPIO.
  • Functionality: As a GPIO, it can be configured as a push-pull output.

Please retest your device and determine which document is correct.

thanks

Matthew

1 reply

ST Technical Moderator
Apr 28, 2026 2:13 PM UTC

Hi @matt-crc 

On STM32N6, PH0 and PH1 are input only as indicated in datasheet not like other products. Actually, these are limited to 1.8V instead of 3.3V

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL