Skip to main content
Associate III
Apr 29, 2025 6:03 PM UTC
Solved

STM32N6 H264 Video Encoder ASIC datasheet / manual

Hello folks,

I am investigating the Video Encoder on the STM32N6 and have been working through the reference project (VENC_SDCard_ThreadX).

The user manual (RM0486) is very vague on detailing the Video Encoder, and lists over 100 pages of registers which appear to be referencing other Software Registers (VENC_SWREGx):

exarian_0-1745948663250.png

There are approximately 500 of registers like these, and it doesn't really say much. 

Looking through the `asicRegisterDesc[]` structure in the Middleware has been useful to try and see what the registers are used for, but still is nowhere near the amount of detail that is needed.

Any further info would be greatly appreciated.

Kindest regards,

 

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
May 7, 2025 1:46 PM UTC

Hello @exarian;

 

I reported the description issue in the reference manual internally.

I advise you to look at Hantro.VC8000NanoE.V50x.SW.Integration.Guide-v1.02-20200708.pdf document may help you.

I recommend you to run an example like VENC_JPEG_Encoding can help you to understand the VENC.

Internal ticket number: 209269 (This is an internal tracking number and is not accessible or usable by customers)

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

11 replies

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
May 7, 2025 1:46 PM UTC

Hello @exarian;

 

I reported the description issue in the reference manual internally.

I advise you to look at Hantro.VC8000NanoE.V50x.SW.Integration.Guide-v1.02-20200708.pdf document may help you.

I recommend you to run an example like VENC_JPEG_Encoding can help you to understand the VENC.

Internal ticket number: 209269 (This is an internal tracking number and is not accessible or usable by customers)

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
Will_Robertson
Associate III
Oct 18, 2025 2:26 PM UTC

Hi Kaouthar @KDJEM.1 and @exarian ,

Thank you very much for this conversation and the link to the H264 encoder documentation and example.

We're planning a new open source wildlife camera system for conservation of Europe's most endangered dormouse, bat and squirrel species which combines the STM32N6 series MCUs and ST image sensors so it's very valuable for us to learn more about the H264 encoder on the STM32N6 series.

>I reported the description issue in the reference manual internally.
>Internal ticket number: 209269 (This is an internal tracking number and is not accessible or usable by customers)

I was wondering if there was any update on this?

Thank you very much,

Will

KDJEM.1
ST Technical Moderator
Oct 20, 2025 6:31 AM UTC

Hello @Will_Robertson ,

 

The 209269 ticket is under investigation.

I recommend you to look at these resources may help you:

Introduction to Hardware Video Encoding with STM32 - stm32mcu

H264 Hardware Handshake encoding - stm32mcu

H264 power consumption setup - stm32mcu

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
exarianAuthor
Associate III
May 7, 2025 2:01 PM UTC

Thank you @KDJEM.1 

That is a great reference to understand the EWL better, I appreciate it.

I have been working with the VENC_SDCard_ThreadX demo, and have managed to encode a video stream, using a test pattern sequence as well as the DCMI.

 

 

Will_Robertson
Associate III
Jun 18, 2026 3:22 PM UTC

Hi ​@KDJEM.1 ,

How are things going with the description in the reference manual for the VENC (internal ticket 209269)?

We're working extensively with the VENC using the existing documentation at the moment and really feeling the need for more in-depth documentation on the features implemented in the VENC on the N6.

It's difficult to use the Hantro VC8000NanoE because it doesn't tell us which Hantro VC8000NanoE features are and aren't implemented in the N6.

Thank you very much for your help.

Will

svogl
Associate III
Jun 19, 2026 10:30 AM UTC

More information would be helpful, please also refer to this ticket -