Skip to main content
Associate II
Jul 22, 2026 8:48 AM UTC
Solved

STM32N6 CSI interface - must be in this case resistor at the CSI output CSI_REXT?

Hi,

In my project with STM32N6 am not using CSI interface, so in this case, all CSI pins are not connected.
But what about CSI output CSI_REXT where according to the manual must be connected 200 Ohm resistor to GND?

Can I keep this pin unconncted too? 
In the manual there is only information that resistor is for setting current for RX/TX driver. 

Similar situation is in USB interfaces, but in STM32N6 Nucleo-144 development board is one of the USB completly unconnected (including OTG2_TXRTUNE pin with similar function like CSI_REXT pin). Which I take as an aswer in case of USB.


I dont know what is diferences in internal structure between RX/TX driver in USB and CSI, but i case of USB in my project (USB is not used too) i wil keep every pins unconnected. But can I afford it in case of CSI?

 

Thanks a lot.

Rddk.

 

FBLBest answer
ST Technical Moderator
Aug 26, 2026 10:54 AM UTC

Hi ​@Rddk 

  1. When I am not using CSI, can I really connect VDDCSI and VDDA18CSI to (VSS) GND? 

Indeed, you can refer to table 5. Auxiliary supplies group in AN5967

  1. And what about CSI_REXT? Where connect it, when am not using CSI? 

All CSI signals must be left floating or all connected to VSS.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

3 replies

ST Technical Moderator
Aug 4, 2026 9:31 AM UTC

Hi ​@Rddk 

Similar question is raised about the same topic in this thread.

CSI_REXT requires a 200Ω resistor to GND with 1% tolerance because it is specific to the CSI PHY IP, which includes a calibration machine relying on this external reference resistor.

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
RddkAuthor
Associate II
Aug 25, 2026 11:42 AM UTC

Hi ​@FBL 
 

Thank you for your aswer, but it only partially answered my questions.

I am sightly confused, in MCU manual and design notes is directly written that VDDCSI must be connected to the same potential as VDDCORE.

When I am not using CSI, can I really connect VDDCSI and VDDA18CSI to (VSS) GND? 
And what about CSI_REXT? Where connect it, when am not using CSI? 

 

Rddk.


 

FBLBest answer
ST Technical Moderator
Aug 26, 2026 10:54 AM UTC

Hi ​@Rddk 

  1. When I am not using CSI, can I really connect VDDCSI and VDDA18CSI to (VSS) GND? 

Indeed, you can refer to table 5. Auxiliary supplies group in AN5967

  1. And what about CSI_REXT? Where connect it, when am not using CSI? 

All CSI signals must be left floating or all connected to VSS.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL