STM32L5xx OctoSPI Read/Write to Xilinx FPGA Configuration Using SelectMAP
Hi. I want to use the OctoSPI to configure Xilinx FPGAs (e.g., Kintex-7) in the SelectMAP mode. Therefore I need 8 data bits, a chip select (CSn), a RD/nWR signal and a CLK to the FPGA. I know the OctoSPI is usually used for reading and writing to QSPI or Octo-Flash memories, which have instruction commands that are passed to the Flash before the actual data transfer occurs. In the case of the Xilinx SelectMAP, it’s more like a FIFO where I just need to set the RD/nWR low (write mode), along with chip select low, then just <write><write><write>…<write> a total of 16 MBytes of data. Conversely, if I wants to read back the FPGA configuration I set the RD/nWR high (read mode), assert CSn low, then just <read><read><read>…<read> all of the 16 MBytes of data back.
Based on the information I’ve read in the STM5L-Series Reference Manual (RM0438), it looks like I may do this in either Indirect- or Memory-Mapped-Mode. So I have four questions:
- Is this possible, to just write (or read) a block of data out of the OctoSPI port without the addition of instructions or commands prior or during the block of data transfer?
2. Is the SPI_DQS used as the RD/nWR signal, or would this be a separate GPIO?
3. Can I use the MCU's DMA engine to do this transfer?
4. Do you have example C-code (or pseudo code) that goes over the OctoSPI configuration and process I would use?
Thanks!