Skip to main content
berendi
Principal
Apr 26, 2020 4:51 PM UTC
Question

STM32L4xx reference manuals System clock (SYSCLK) selection

RM0351 and RM0392 (and maybe others, haven't checked them all) contain this in the System clock (SYSCLK) selection section

Status bits in the Internal clock sources calibration register (RCC_ICSCR) indicate which clock(s) is (are) ready and which clock is currently used as a system clock.

However the various clock ready and system clock switch status bits are actually located in RCC->CR and RCC->CFGR.

This topic has been closed for replies.

2 replies

ST Technical Moderator
Apr 27, 2020 2:22 PM UTC

Hello,

I raised this internally for update.

Thank you for your contribution.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
waclawek.jan
Super User
Apr 27, 2020 7:14 PM UTC

Hi @Imen DAHMEN​ ,

I've seen the same sentence also in RM0440 and RM0444, so this propagates across families.

Jan