STM32L4R9AII6 generates 16 SPI clock pulses when I have selected data size 8 in STM32CubeMX.
STM32L4R9AII6 generates 16 SPI clock pulses when I have selected data size 8 in STM32CubeMX.
When I measure the SPI clock when I write a single byte to the SPI1 DR register it outputs 16 clocks.
When I debug I can look at the SPI1 registers. The CR2 DS bits = 7. According to the datasheet this is 8 bits. But when I measure there is 16 clocks when I write a single byte to the DR register.
If I change the DS bit to 3 it will output 8 bits.
What is going on?