STM32L4A6VGT power consumption?
Hi,
I am measuring a STM32L4A6VGT board power consumption. From the datasheet, in standby mode should be 120nA while I got the value @ 19 mA (last Friday). The FW does nothing, in main after MX_XXX init, call HAL_PWR_EnterSTANDBYMode(). Now I am getting 2.4 mA (not sure what actually make the value changed. It's early Monday morning).
My question is "is there any functions I should call (maybe turnoff bus, clock...etc) before going to low power such as standby mode?"
Why am I getting such big number compare with the datasheet?
Thx
– 30 nA Shutdown mode (5 wakeup pins)
– 120 nA Standby mode (5 wakeup pins)
– 420 nA Standby mode with RTC