Skip to main content
Associate III
Aug 12, 2026 2:47 PM UTC
Question

STM32L496RGT6 UART sourcing current capacity

Hi,

We have configured PB11 and PC4 for UART. when UART send data, what is pin current sourcing capacity?

/Anurag

 

 

2 replies

Andrew Neil
Super User
Aug 12, 2026 3:01 PM UTC

See the datasheet for the GPIO specifications - it’s not specific to what Alternate Function is used (eg, UART).

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Gyessine
ST Technical Moderator
Aug 13, 2026 9:49 AM UTC

Hello ​@Anuraglokhande 
It is stated in the product datasheet Output driving current section that The GPIOs (general purpose input/outputs) can sink or source up to ±8 mA, and sink or source up to ± 20 mA (with a relaxed VOL/VOH). GPIOs PC13, PC14 and PC15 are supplied through the power switch, limiting source capability up to 3 mA only.
You can review the datasheet for more details
BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.