Skip to main content
Associate III
Nov 5, 2026 1:21 PM UTC
Question

STM32L496 Low Power Run Mode

Hi,

We are using STM32L496. We are trying with Dynamic voltage scaling is being used and set to Range 2 and Low-power run mode. 

MCU is connected with 1.2V at VDD12 with external SMPS. 

How do we know, MCU is taking power from VDD12 SMPS or main VDD rail?

VDD = 2.5V

/Anurag

 

 

3 replies

ST Technical Moderator
Nov 6, 2026 10:46 AM UTC

Hi ​@Anuraglokhande 

Can you provide full ordering information? or part number to check whether the device has the external SMPS capable pinout.

Standard devices use the integrated LDO. P suffix variants include VDD12 pins that can provide a path to VCORE and bypass the internal LDO when an external SMPS is used.

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Associate III
Nov 6, 2026 10:49 AM UTC

Hi,

 

Please note,

MPN: STM32L496RGT6P

 

So this device still usage supply at VDD12 from external SMPS in Low-power run mode?

 

Are there two LDO inside MCU, as mentioned in datasheet, but not in architecture. 

→ Two embedded linear voltage regulators supply most of the digital circuitries: the main regulator (MR) and the low-power regulator (LPR).

 

/Anurag

 

ST Technical Moderator
Nov 6, 2026 5:22 PM UTC

Hi ​@Anuraglokhande 

P suffix identifies the version with VDD12 pins for an external SMPS connection. It does not mean the external SMPS supplies the core in every operating mode. VDD12 can be externally forced, but not in every power mode.

As specified in RM0351, the external SMPS should be connected through a GPIO controlled load switch.

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL