Skip to main content
Associate III
Jun 15, 2026 7:31 AM UTC
Solved

STM32L476RCTX for audio application.

Hi,

 

Can I use DAC of STM32L476RCTX for audio application. I have to give output of DAC to MAX97220(Audio amplifier IC). 

Frequency range of audio is 10Hz to 20kHz. 

Can you please suggest any application note for this. 

Audio files will be fetched from SD card with SPI interface.

Can you please suggest any code example or library that is already available for this type of example. 

 

Regards,

Anurag

 

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jun 15, 2026 3:59 PM UTC

Hello,

Please refer to the AN3126 “How to use DAC for audio and waveform generation on STM32 MCUs and MPUs”

Hope that helps

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jun 15, 2026 3:59 PM UTC

Hello,

Please refer to the AN3126 “How to use DAC for audio and waveform generation on STM32 MCUs and MPUs”

Hope that helps

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.