Question
STM32L476 USB_OTG can't get recognized by Windows
Posted on January 25, 2018 at 21:23
Version:1.0 StartHTML:0000000168 EndHTML:0000000993 StartFragment:0000000435 EndFragment:0000000976
I have configured the USB_OTG as a mass storage on STM32L476VE that has a 8MHz external crystal, and when I connect it to windows computer it can't recognize it. I have read on the boards that some other people are also having similar problems and saying that the problem is related to the HAL_USB driver. I have updated the MXCube and eclipse software. Is there any update to the driver, or any patch or update?
Thanks,