STM32L476 bus fault escalated hard fault in HAL uart_irq() when spamming USART2
Hi all,
Our team is developing on a custom PCB with STM32L476. And we are testing our CLI robustness, we found out that when we spam the CLI which uses USART2 at baud rate 115200, the program goes into hard fault. Upon investigating with a JLINK debugger, and looking at CFSR, we found we have precise bus fault. And the PC and LP both point to the function uart_irq() in serial_device.c. specifically line 0x080331b8:
if (__HAL_UART_GET_FLAG(huart, UART_FLAG_TXE) != RESET) {
0x080331b4 ldr r3, [sp, #16]
0x080331b6 ldr r3, [r3, #0]
0x080331b8 ldr r3, [r3, #28] which is accessing USART_TypeDef's ISR attribute. And as the image shown below, R3+#28 is the memory address stored in BFAR.

We've also found a post that might be relevant to this problem we are facing, but it happened on STM32F. And upon looking at USART2's register ISR, we found the ORE flag is tripped. And we are also using mbedOS on top of HAL if that matters.
Does anyone know why this is happening? And if this can be fixed? Thank you all.