STM32L475RE Connection lost
Hello together,
I am currently trying to program a STM32L475RET6. But I have the problem that when I connect the programmer and click on connect, a connection can be established, but it disappears after only a short time with the error "connection lost".
I have already made a few designs and projects with the L4, but never observed such behavior. Has anyone been able to observe this behavior?
Message from STM32Cube Programmer:
06:57:38 : UR connection mode is defined with the HWrst reset mode
06:57:38 : ST-LINK SN : 0036004F3331511934333834
06:57:38 : ST-LINK FW : V3J10M3B5S1
06:57:38 : Board : STLINK-V3SET
06:57:38 : Voltage : 3.29V
06:57:38 : SWD freq : 8000 KHz
06:57:38 : Connect mode: Normal
06:57:38 : Reset mode : Hardware reset
06:57:38 : Device ID : 0x415
06:57:38 : Revision ID : Rev 4
06:57:38 : Debug in Low Power mode enabled.
06:57:38 : UPLOADING OPTION BYTES DATA ...
06:57:38 : Bank : 0x00
06:57:38 : Address : 0x40022020
06:57:38 : Size : 20 Bytes
06:57:38 : Bank : 0x01
06:57:38 : Address : 0x40022044
06:57:38 : Size : 16 Bytes
06:57:38 : UPLOADING ...
06:57:38 : Size : 1024 Bytes
06:57:38 : Address : 0x8000000
06:57:38 : Read progress:
06:57:38 : Data read successfully
06:57:38 : Time elapsed during the read operation is: 00:00:00.002
06:57:40 : Error: Unable to get core ID
06:57:40 : Error: Unable to get core ID
06:57:40 : Error: Unable to get core ID
06:57:40 : Warning: Connection to device 0x415 is lost
06:57:40 : Disconnected from device.