Skip to main content
adrian
Associate III
November 27, 2018
Question

STM32L475RC RTC Issue?

  • November 27, 2018
  • 3 replies
  • 928 views

Are there any known issues with the RTC Wakeup on the STM32L475?

I cannot get it to work, I've copied the code exactly as it appears in the STOP2_PWR example, but no matter what I do the ISR does not get called.

If I check the registers I can see the the wakeup timer has elapsed, the interrupt is enabled.

I'm totally at a loss here.

I did ask about a week ago, but have had no response.

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
November 27, 2018

ST Staff would need to be contacted via the FAE supporting your project, or the Online Support Request.

Not an area I've had cause to dig into at this point.

https://community.st.com/s/question/0D50X0000A1k8fJSQQ/halrtcexsetwakeuptimerit-issue-stm32l475rc

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
adrian
adrianAuthor
Associate III
November 27, 2018

Hi,

we’ve contacted our supplier to get fae support, I really am lost as to why this isn’t working. I have used the RTC wake up on other STM32 series without any problems, but this just refuses to work.

Jocelyn RICARD
ST Employee
December 3, 2018

Hello Adrian,

I got the request from online support, so I update here to share with all.

The issue as I've seen is related to a regression in latest HAL RTC driver. A specific update was done to introduce STM32F412, and one line of code was changed for some reason:

You can see this in the code of HAL_RTCEx_SetWakeUpTimer_IT function:

__HAL_RTC_WAKEUPTIMER_EXTI_ENABLE_IT

was replaced by

__HAL_RTC_WAKEUPTIMER_EXTI_ENABLE_EVENT

So, when calling the the function HAL_PWREx_EnterSTOP2Mode you should give

PWR_STOPENTRY_WFE instead of PWR_STOPENTRY_WFI

I raised this regression to the development teams.

I'm sorry for the inconvenience.

Best regards

Jocelyn