Associate II
September 19, 2022
Question
STM32L471RET6 Strange interaction about PB12 and PC12
- September 19, 2022
- 3 replies
- 975 views
Hello all, I have encountered unexpected behavior on the voltage level of PC12 when I enable PB12.
My setup:
PC12: Level high, output mode PP, no PU no PD, Output speed High.
PB12: Level low, output mode PP, no PU no PD, Output speed Low.
Without PB12 the High level of PC12 reaches 3.3V, enabling PB12 its high value becomes max 1.46V.
In my application PC12 was used as a chip select in an SPI comunication, It has a hardware pull up of 100K; PB12 was used for debugging purposes