Skip to main content
damh
Associate III
Jun 20, 2017 3:43 PM UTC
Question

STM32L471 WFI problem

Posted on June 20, 2017 at 17:43

On STM32L471 (DEV_ID=0x6415, REV_ID=0x1007)

~4% of mcus do not enter standbymode and ignore the WFI instruction.

Does anyone have ideas how to get it working on all mcus? (tested with 150 pieces)

Is there any known bug/problem?

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    Jun 20, 2017 4:37 PM UTC
    Posted on June 20, 2017 at 18:37

    Are you looping on the WFI instruction? Anything driving NRST?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    damh
    damhAuthor
    Associate III
    Jun 20, 2017 7:05 PM UTC
    Posted on June 20, 2017 at 19:05

    yes, it's the cube function [HAL_PWR_EnterSTANDBYMode()]

    NRST has an external pullup (10k) and capacitor (100nF) to GND.

    In one case NRST is connected additionally to the debugger or in second case open, but there is no difference.

    All other units (144 pcs.) work correctly with the same firmware.

    damh
    damhAuthor
    Associate III
    Jun 23, 2017 3:05 PM UTC
    Posted on June 23, 2017 at 17:05

    Is there a way to determine, why the wfi command is ignored? What flags have to be checked?