Question
STM32L471 ADC offset 0.1V?
The CPU is powered using 1.8V both on VDD as well as VDDA (4.7uH coil as well as 1n/100n/1u capacitors in power path).
When I measure the Vbat pin (100n cap supporting) in the range 2V-3.6V using the ADC I always measure about 0.1V less than the voltage as measured by my lab equipment.
Where does this offset originate from? I find nothing in AN2834 that would correspond to such a high error (it is like 228 LSB)