Skip to main content
Riscy00_UPP
Associate II
April 27, 2023
Question

STM32L452CC and STM32L4Q5CGU6, issue with USART

  • April 27, 2023
  • 3 replies
  • 1402 views

My colleagues went to my office and reported that the STM32L452CC with the USART interface (5MHz and 10MHz) was working fine but had to use STM32L4Q5CG due to stock usage, but it failed at 10MHz but working fine 5MHz.

I have explored errata, datasheet and reference manual (L452 and L4Q5), and I don't see anything obvious to explain why 10MHz USART (in UART mode via RS485 transceiver) is not working on STM32L4Q5CG.I wonder if you may shed some light on what to look for in the firmware that is causing this issue or if something is missing from Errata.

Thanks

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
April 28, 2023

Not working is a bit non-specific.

What is happening? Getting some data? Scope or Logic Analyzer can see correct data, at correct frequency? Problem receiving or transmitting?

Clocking the parts / buses differently? What frequencies?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Riscy00_UPP
Associate II
April 28, 2023

Yes it is non-specific,I was hoping for some pinpointing of what actual changes between MCU of the very same specs under the same reference manuals, that stop 10MHz from working.

Tesla DeLorean
Guru
April 28, 2023

Ones an L4 at 80 MHz, the other is an L4+ at 120 MHz, so different die for sure.

Probably different IRQ and DMA relationships.

Going to need to isolate what aspects are and are not functioning

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..