Skip to main content
Associate
Sep 5, 2025 1:18 PM UTC
Question

STM32L451VETR: DAC output drops to 0 after BOR event in STOP2 mode

 

I am facing a strange issue that looks like a possible microcontroller design/behavior problem.

My setup:

  • I need the DAC output pin to provide a stable voltage while the microcontroller is in STOP2 sleep mode with the RTC running.

  • Power connections: Vbat, Vdda, and Vref are connected to Vdd.

  • An additional external supervisor is used: MCP130T-270I/TT.

Problem description:

  • Initially, everything works fine — the DAC output stays at the expected voltage in STOP2 mode.

  • However, after a BOR (Brown-Out Reset) occurs, the behavior changes: when the microcontroller enters STOP2 mode, the DAC output pin drops to 0V.

  • After this happens:

    • Resetting the microcontroller does not fix it.

    • Power-cycling the device also does not fix it.

  • The only way to recover normal DAC behavior is to connect via debugger.

Has anyone experienced similar behavior? Could this be a silicon bug, or am I missing some configuration after BOR?

 

My DAC config:

sConfig.DAC_SampleAndHold = DAC_SAMPLEANDHOLD_ENABLE;
sConfig.DAC_SampleAndHoldConfig.DAC_HoldTime = 10;
sConfig.DAC_SampleAndHoldConfig.DAC_RefreshTime = 10;
sConfig.DAC_SampleAndHoldConfig.DAC_SampleTime = 10;
sConfig.DAC_Trigger = DAC_TRIGGER_NONE;
sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;
sConfig.DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_DISABLE;
sConfig.DAC_UserTrimming = DAC_TRIMMING_FACTORY;
if (HAL_DAC_ConfigChannel(&hdac1, &sConfig, DAC_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}

void sleep(void)
{
HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0xA000, RTC_WAKEUPCLOCK_RTCCLK_DIV16);
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
}
Test case:
HAL_DAC_Start(&hdac1, DAC_CHANNEL_1);
HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_R, 1000);
sleep();
HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_R, 2000);
sleep();

 

 

This topic has been closed for replies.

2 replies

TDK
Sep 5, 2025 1:33 PM UTC

A power cycle doesn't fix it? What else on the board is connected to DAC1?

Why is a BOR occurring at all if an external supervisor is being used?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Pawel_SAuthor
Associate
Sep 5, 2025 1:55 PM UTC

Yes, power cycle doesn't fix it, even I short a capacitors on MCU to discharge everything.
DAC1 output is connected to external amplifier input.

I added:
if (__HAL_RCC_GET_FLAG(RCC_FLAG_BORRST))
{
__HAL_RCC_CLEAR_RESET_FLAGS();
__HAL_RCC_BACKUPRESET_FORCE();
asm("nop");asm("nop");asm("nop");asm("nop");asm("nop");
__HAL_RCC_BACKUPRESET_RELEASE();
led_red_on();
HAL_Delay(1000);
NVIC_SystemReset();
}

and the red led is on after power up.

Only when I connect/disconnect in CubeProgrammer then everything returns to normal operation.