Skip to main content
MDebu.1
Associate
March 4, 2022
Solved

STM32L451RC are there Problems known for the BSDL File? I tried to do a Boundary Scan but it is not possible to set the Pins I want. I try to write 334 Bit but If I change the state ob a Pin from outside, I see that this Pin appears 120 Cells before.

That is what I send for exsample:

SIR 9 TDI (0);

SDR 334 TDI (49000000001249240a49249248000000000001249200000000000249249249008000000001249200) SMASK (3fffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffffff) TDO (0) MASK (0);

This topic has been closed for replies.
TZARDI
TZARDIBest answer
Visitor II
April 1, 2022

Hello,

I confirm that there is an issue with the STM32L451_LQFP64.bsd package, thanks for bringing it to our attention..

An internal ticket number 125629  (This is an internal tracking number and is not accessible or usable by customers) has be logged to check all the other packages.

Please find attached an updated version of the needed file.

Please note that an updated version of the file en.stm32l4_bsdl will be available on ST website.

6 replies

TZARDI
Visitor II
March 23, 2022

Hello,

Can you please precise the package you're using?

Br,

MDebu.1
MDebu.1Author
Associate
March 23, 2022

Package is LQFP64

I Took the BSDL File for the Package STM32L451_LQFP64.bsd and than the Cortex

TZARDI
Visitor II
March 29, 2022

Hello,

The BSDL chain length is 234 bits long. And it seems that you're shifting 334 bits

Can you check that? an is the STM32 daisy-chained with other devices?

Br,

MDebu.1
MDebu.1Author
Associate
March 29, 2022

Thank you for your Answer, it is difficult to check without the right BSDL File. I use the File witch is available at the st homepage like specified before, with the zip File en.stm32l4_bsdl. Downloaded a few Weeks before. In the bsdl File the JTAG Interface is specified with 333 Cells (0 till 332). The File is dated with 09-May-2017. Obviously you have an other BSDL File. Can you provide a link to the File? There are no other devices in the scan chain (Except the Cortex TAP).

TZARDI
TZARDIBest answer
Visitor II
April 1, 2022

Hello,

I confirm that there is an issue with the STM32L451_LQFP64.bsd package, thanks for bringing it to our attention..

An internal ticket number 125629  (This is an internal tracking number and is not accessible or usable by customers) has be logged to check all the other packages.

Please find attached an updated version of the needed file.

Please note that an updated version of the file en.stm32l4_bsdl will be available on ST website.

MDebu.1
MDebu.1Author
Associate
April 6, 2022

Thank you for your support!!!