Skip to main content
RStra
Associate III
May 4, 2020
Solved

STM32L433 VREFINT_CAL Value

Hello,

I'm trying to work with the ADC of the STM32L433 microcontroller. The Reference manual (RM0394) on page 448 it says :

The following formula gives the actual VDDA voltage supplying the device:

VDDA = 3.0 V x VREFINT_CAL / VREFINT_DATA

Where can I found the VREFINT_CAL value, I'm not able to find the address on the RM ?

Thank you

Riccardo

This topic has been closed for replies.
TDK
TDKBest answer
May 4, 2020

It's in the datasheet. Note that it's called VREFINT here instead of VREFINT_CAL.

0693W000000Wr32QAC.png

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
May 4, 2020

It's in the datasheet. Note that it's called VREFINT here instead of VREFINT_CAL.

0693W000000Wr32QAC.png

"If you feel a post has answered your question, please click ""Accept as Solution""."
PR.10
Associate III
February 29, 2024

I was confused by naming mismatch too :thinking_face:. For people from future, there are actually a built in macros for that which do have matching names. So the code can stay correct when you change mcu variant. in *adc.h

 

 

/* ADC internal channels related definitions */
/* Internal voltage reference VrefInt */
#define VREFINT_CAL_ADDR ((uint16_t*) (0x1FFF75AAUL)) /* Internal voltage reference, address of
 parameter VREFINT_CAL: VrefInt ADC raw data acquired at temperature 30 DegC
 (tolerance: +-5 DegC), Vref+ = 3.0 V (tolerance: +-10 mV). */
#define VREFINT_CAL_VREF ( 3000UL) /* Analog voltage reference (Vref+) value
 with which VrefInt has been calibrated in production
 (tolerance: +-10 mV) (unit: mV). */