Skip to main content
Skadi F
Associate II
June 14, 2018
Question

STM32L433: Using PH0 PH1 as GPIO

Posted on June 14, 2018 at 12:12

Hi,

I realized a prototype including the STM32L433 (LQFP64 package). I tried to use the pins PH0 and PH1 as OUTPUT pins. This should be possible according to the datasheet (5V tolerant I/O pins). This pins can be used to attach a crystal or oscillator to the controller. This external clock would act as

HSE

, which I do not use (haven't installed). So disabled the HSE as well as the LSE.

I wasn't able to set the pins PH0 and PH1 HIGH. Interestingly, for the pins PC14 and PC15, which are responsible for the

LSE

, it works fine. I defined the pins PH0, PH1, PC14 and PC15 in as push-pull outputs.

Is it possible to use PH0 & PH1 as GPIO pins, or have I missed something in the datasheet?

BR

#hse #stm32l433 #gpio #push-pull #output
This topic has been closed for replies.

6 replies

Tesla DeLorean
Guru
June 14, 2018
Posted on June 14, 2018 at 12:19

Can't say I've dug into the L4 data in this regard, other STM32 including the L0 allow for OSC_IN/OSC_OUT to be retasked as GPIO, might want to check the bits in the RCC registers, as those take precedence over GPIO/AF settings.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
TDK
June 15, 2018
Posted on June 15, 2018 at 21:11

This is for the STM32F4, but it's likely the same for you.  From the reference manual:

8.3.14 Using the OSC_IN/OSC_OUT pins as GPIO PH0/PH1 port pins

The HSE oscillator pins OSC_IN/OSC_OUT can be used as general-purpose PH0/PH1 I/Os, respectively, when the HSE oscillator is OFF. (after reset, the HSE oscillator is off). The PH0/PH1 I/Os are only configured as OSC_IN/OSC_OUT HSE oscillator pins when the HSE oscillator is ON. This is done by setting the HSEON bit in the RCC_CR register. The HSE has priority over the GPIO function.

Double check that it's actually disabled.  And see what the STM32L4 manual has to say on the matter.

"If you feel a post has answered your question, please click ""Accept as Solution""."
waclawek.jan
Super User
June 15, 2018
Posted on June 15, 2018 at 23:03

DId you read back the relevant RCC and GPIOH registers and check if they were set as you expected?

JW

Skadi F
Skadi FAuthor
Associate II
June 17, 2018
Posted on June 17, 2018 at 12:40

Hi, I'm using ChibiStudio, I tried to check the register by the debugging the controller with OpenOCD. Unfortunatly I'm not able to debug the controller. I tried to use the stm32l4discovery.cfg file, but it doesn't work. By using stm32ldiscovery.cfg file the configuration seems to work, althoug the wrong controller is detected: stm32l1.cpu: hardware has 6 breakpoints, 4 watchpoints. By performing the debugging process, a pop up window appears with following massage: Target request failed: Don't know how to run. Try 'help target'.

Nevertheless, I disabled the HSE twice. Once in the config file and a second time in the main file by: 

RCC->CR &= ~RCC_CR_HSEON;            // Disable HSE

GPIOH -> MODER &= 0x00000005;         // PH0 & PH1: OUTPUT; default: 0x0000000F

GPIOH -> OTYPER &= 0x00000000;        // Output push-pull (reset state); default: 0x00000000

GPIOH -> ODR |= 0x00000003;                 // set PH0 & PH1 initial HIGH

Without any success.

TDK
June 17, 2018
Posted on June 17, 2018 at 20:13

What are your clock settings?

It's going to be hard to debug issues without a reliable debug mechanism.  Can you send text to a terminal using a UART or something?  You could also blink an onboard LED as a (very limited) debug mechanism.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Skadi F
Skadi FAuthor
Associate II
June 17, 2018
Posted on June 17, 2018 at 20:46

Hi,

I enabled the HSI @ 16 MHz, LSI @ 32 kHz and I also use the 48 MHz internal clock, which is used for USB communication. The PLL source is the 16 MHz HSI, PLL_M = 4, PLL_N = 40, PLL_R = 2, and of course the system clock mux input is the PLL clock. Resulting in a system clock of 80 MHz.

The controller it self works fine so far. I'm able to communicate via USB and a LED is attached to a GPIO pin. I'm able to switch the LED on and off via serial/USB commands.

The only thing which doesn't work so far, is the usage of the PH0 and PH1 as push-pull outputs.

BR