Skip to main content
Peter Mather
Associate III
Dec 13, 2018 7:33 PM UTC
Solved

STM32L433: can't make sense of Flash Loader Demonstrator

During development I've been using ST-LInk to program the STM32L433 which of course works perfectly. I want to release the firmware and allow users to be able to update the code over UART2.

I've set BOOT0 and can see the device using the latest version of the STM Flash Loader Demonstrator program (V2.8.0). It reports PID = 435, BID = NA, Version 3.1. The flash mapping panel is completely blank. It says it is read protected although I haven't set any protection.

I can use the option to disable read protection and this seems to work - I get the message "Read protection was successfully removed" but if I try to read the chip it again says it is read protected. If I try and erase or write the chip I always get the read-protected message.

I'm missing something as usual but what?

Help gratefully appreciated

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Dec 13, 2018 10:00 PM UTC

Use the STM32 Cube Programmer, it has a USART mode, the old software is deprecated/abandoned.

https://www.st.com/en/development-tools/stm32cubeprog.html

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

1 reply

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Dec 13, 2018 10:00 PM UTC

Use the STM32 Cube Programmer, it has a USART mode, the old software is deprecated/abandoned.

https://www.st.com/en/development-tools/stm32cubeprog.html

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..