Skip to main content
Ivo
Associate II
Dec 2, 2020 1:23 PM UTC
Solved

STM32L432KC RTC wakeup from STOP1 mode not working.

The processor never wakes up from STOP1 mode and I do not know why.

Reading RTC time and date works, so I know the RTC clock is running. With debugger (using HAL_EnableDBGStopmode()), I notice that the firmware is stuck in __WFI()

I'm using STM32Cube_FW_L4_V1.13.0

static void deepsleep(uint32_t intervalms)
{
 __HAL_RCC_PWR_CLK_ENABLE(); // Enable Power Control clock
 
 HAL_RTCEx_BKUPWrite(&hrtc, RTC_BKP_DR1, 0x32F2);
 HAL_NVIC_EnableIRQ(RTC_WKUP_IRQn);
 
 if (HAL_RTCEx_DeactivateWakeUpTimer(&hrtc) != HAL_OK) {
 Error_Handler();
 }
 
 // clear wake up flags
 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
 __HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF);
 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUFI);
 
 uint32_t _time = (intervalms * 2314) / 1000;
 if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, _time, RTC_WAKEUPCLOCK_RTCCLK_DIV16) != HAL_OK) {
 Error_Handler();
 }
 
 HAL_SuspendTick();
 HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
 // Issue: remains stuck in __WFI(), never wakes up
 HAL_ResumeTick();
 
 // Reinit clocks
 SystemClock_Config();
 // Deactivate RTC wakeUp
 if (HAL_RTCEx_DeactivateWakeUpTimer(&hrtc) != HAL_OK) {
 Error_Handler();
 }
}
 
int main(void)
{
 HAL_Init();
 SystemClock_Config();
 // For debugging:
 HAL_EnableDBGStopMode();
 MX_GPIO_Init();
 MX_RTC_Init();
 while (1)
 {
 HAL_GPIO_WritePin(LD3_GPIO_Port, LD3_Pin, GPIO_PIN_SET);
 HAL_Delay(1000);
 HAL_GPIO_WritePin(LD3_GPIO_Port, LD3_Pin, GPIO_PIN_RESET);
 deepsleep(1000);
 }
}
 
**
 * @brief RTC Initialization Function
 * @param None
 * @retval None
 */
static void MX_RTC_Init(void)
{
 
 /* USER CODE BEGIN RTC_Init 0 */
 
 /* USER CODE END RTC_Init 0 */
 
 RTC_TimeTypeDef sTime = {0};
 RTC_DateTypeDef sDate = {0};
 
 /* USER CODE BEGIN RTC_Init 1 */
 
 /* USER CODE END RTC_Init 1 */
 /** Initialize RTC Only 
 */
 hrtc.Instance = RTC;
 hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
 hrtc.Init.AsynchPrediv = 127;
 hrtc.Init.SynchPrediv = 255;
 hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
 hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
 hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
 hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
 if (HAL_RTC_Init(&hrtc) != HAL_OK)
 {
 Error_Handler();
 }
 
 /* USER CODE BEGIN Check_RTC_BKUP */
 
 /* USER CODE END Check_RTC_BKUP */
 
 /** Initialize RTC and set the Time and Date 
 */
 sTime.Hours = 0x0;
 sTime.Minutes = 0x0;
 sTime.Seconds = 0x0;
 sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
 sTime.StoreOperation = RTC_STOREOPERATION_RESET;
 if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
 {
 Error_Handler();
 }
 sDate.WeekDay = RTC_WEEKDAY_MONDAY;
 sDate.Month = RTC_MONTH_JANUARY;
 sDate.Date = 0x1;
 sDate.Year = 0x0;
 
 if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
 {
 Error_Handler();
 }
 /** Enable the WakeUp 
 */
 if (HAL_RTCEx_SetWakeUpTimer(&hrtc, 0, RTC_WAKEUPCLOCK_RTCCLK_DIV16) != HAL_OK)
 {
 Error_Handler();
 }
}
 

This topic has been closed for replies.
Ivo
IvoBest answer
Associate II
Dec 3, 2020 4:45 PM UTC

After updating to STM32Cube_FW_L4_V1.16.0, that is.

4 replies

waclawek.jan
Super User
Dec 2, 2020 8:14 PM UTC

Okay, and without entering sleep, does the respective interrupt fire?

JW

Ivo
IvoAuthor
Associate II
Dec 3, 2020 10:54 AM UTC

No, without entering STOP1 mode, interrupt also does not fire.

Reading out time and date every second while waiting in vain for the interrupt does see the RTC time advancing every second.

But HAL_RTCEx_GetWakeUpTimer() stays as-is.

Ivo
IvoAuthor
Associate II
Dec 3, 2020 2:46 PM UTC

It seems like this was a bug in the STM32Cube_FW_L4_V1.13.0 that I was using; after updating to STM32Cube_FW_L4_V1.13.0, I'm getting interrupts.

In V1.13.0, the ST's HAL library was doing "  __HAL_RTC_WAKEUPTIMER_EXTI_ENABLE_EVENT();" in HAL_RTCEx_SetWakeUpTimer_IT(), and in later versions it is doing " __HAL_RTC_WAKEUPTIMER_EXTI_ENABLE_IT();" instead.

Ivo
IvoAuthorBest answer
Associate II
Dec 3, 2020 4:45 PM UTC

After updating to STM32Cube_FW_L4_V1.16.0, that is.