Skip to main content
krestan
Associate II
May 15, 2017 6:07 PM UTC
Solved

STM32L432 flash loader demonstrator

Posted on May 15, 2017 at 20:07

I'd like to ask if there will be any support for STM32L432 for the flash loader demonstrator. So far with the GUI version this device is not supported. I've tried to create STmap file from the STM32L4 just by editting the PID, but for GUI version the device is still not recognized and for the command line version it just recognize the device, but the erasing does not work and with option 'skip 0xFF' is this tool making windows exception and crashes. I'm using the latest version 2.8.0.

#stm32l432-flash-loader-demonstrator
This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Dec 31, 2018 3:55 PM UTC

The software is deprecated. Use the STM32 Cube Programmer, it supports USART/COM connectivity.

https://www.st.com/en/development-tools/stm32cubeprog.html

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

3 replies

ST Technical Moderator
May 16, 2017 7:54 AM UTC
Posted on May 16, 2017 at 09:54

Hello

,

You find attached a newer version of the FlashLoader supporting new devices.

Please try it and keep me informed if it is working as expected or you faced any issue using it.

Thanks

Imen

________________

Attachments :

STMFlashLoader Demo_V2.9.0RC4.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyfT&d=%2Fa%2F0X0000000bAk%2F20oFV9mWzh4rqrQe1SKx.2I.wkjg42k8R4.djml7vcU&asPdf=false
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
jcart
Visitor II
Dec 31, 2018 3:22 PM UTC

Hello,

This version crash also on my comuter.

  • Nom de l’application défaillante STMFlashLoader Demo.exe, version : 2.8.0.0, horodatage : 0x57484afb
  • Nom du module défaillant : ntdll.dll, version : 10.0.17134.471, horodatage : 0xfe852bc4
  • Code d’exception : 0xc0000005
  • Décalage d’erreur : 0x00047ca6
  • ID du processus défaillant : 0x8e8
  • Heure de début de l’application défaillante : 0x01d4a11aa4f7bf82
  • Chemin d’accès de l’application défaillante : C:\Users\jeanc\OneDrive\Documents\Pro-face\flash-loader 8439\STMFlashLoader Demo.exe
  • Chemin d’accès du module défaillant: C:\WINDOWS\SYSTEM32\ntdll.dll
  • ID de rapport : 4f61bcab-b7db-4c55-9bd1-6f617e08a4f6
  • Nom complet du package défaillant :
  • ID de l’application relative au package défaillant :

Do you have any idea ?

Jean C

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Dec 31, 2018 3:55 PM UTC

The software is deprecated. Use the STM32 Cube Programmer, it supports USART/COM connectivity.

https://www.st.com/en/development-tools/stm32cubeprog.html

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..