STM32L431: Enable USART rises IDLE ISF
Hi all,
I'm using the STM32L431RB device and wanna implement UART communication with DMA and IDLE line interrupt functionality. In principle everything is working with one exception:
After enabling USART the IDLE flag in ISR register is set to 1. After that I try to reset that flag by writting a 1 to the corresponding ICR bit, but the IDLE flag is not reset. So I'm running in IDLE ISR directly after initializing the transfer...
It works all fine if I'm implementing a wait function before reseting the IDLE flag.
Can anyone help to avoid the initial ISR call?