Skip to main content
Associate II
Feb 17, 2025 3:47 PM UTC
Solved

STM32L431: Enable EXTI on a Pin Number Used as UART RX on a Different Port

Hello,

I would like to configure PA11 as an EXTI pin. I know that there exists the hardware limitation that there cannot exist two pins with the same pin number in different ports configured as an EXTI pin (I.E., I could not configure both PB11 and PA11 as EXTI inputs). PB11 is already configured as a UART RX pin. Will there be any conflict if I now attempt to configure PA11 as an EXTI input pin, I.E. a low bit being received by PB11 triggers the EXTI interrupt on pin 11? Or does this conflict only occur when two pins of the same number are both configured as EXTI inputs? 

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Feb 17, 2025 3:51 PM UTC

Hello,

No. There is no relation between UART Rx and EXTI interrupt. These lines are totally different. No risk to get EXTI triggered by the UART Rx.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

2 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Feb 17, 2025 3:51 PM UTC

Hello,

No. There is no relation between UART Rx and EXTI interrupt. These lines are totally different. No risk to get EXTI triggered by the UART Rx.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
TDK
Feb 17, 2025 4:26 PM UTC

Furthermore, it is not possible to configure two pins of the same number as EXTI inputs.

"If you feel a post has answered your question, please click ""Accept as Solution""."