Skip to main content
Patrice Favreau
Associate
April 30, 2018
Question

STM32L4 VDD vs VDDUSB vs VDDA

  • April 30, 2018
  • 4 replies
  • 1221 views
Posted on May 01, 2018 at 00:12

I am designing with a STM32L4 in QNF48 and would like to save power...

How about

    VDDUSB = 3.3V

    VDDA = 3.3V with linear regulator , VREF = VDDA

    VDD = 1.8V 

    Now the data sheets say  |∆VDDx| must be less than 50mv .

    

    Is this mean all power need to be at the same level +/- 50mv, or that all of the same name need to be within 50mv

 Thanks!!!

    This topic has been closed for replies.

    4 replies

    waclawek.jan
    Super User
    May 1, 2018
    Posted on May 01, 2018 at 10:01

    Now the data sheets say  |∆VDDx| must be less than 50mv .

    Which datasheets? And how do they exactly describe what |∆VDDx| is?

    JW

    Patrice Favreau
    Associate
    May 1, 2018
    Posted on May 01, 2018 at 10:55

    Every STM32 datasheet I ever saw.

    So if this is true that all vdd need to be basically the same voltage

    Can we use the USB while vdd is not 3.3V?

    Thanks

    waclawek.jan
    Super User
    May 1, 2018
    Posted on May 01, 2018 at 19:55

    Every STM32 datasheet I ever saw.

    Show (you can paste pictures here).

    JW

    Jismal Jamal
    Associate II
    May 11, 2018
    Posted on May 11, 2018 at 09:03

     |∆VDDx| must be less than 50mv  :- Variations between different VDDX power pins of  the same domain

    So if VDDIO2 ,VDD ,VDDUSB are of separate domains so no issue as of my knowledge correct me if i am wrong.