Skip to main content
Dilbert K
Associate III
September 22, 2017
Question

STM32L4 USBD receive

  • September 22, 2017
  • 1 reply
  • 515 views
Posted on September 22, 2017 at 15:45

I am currently using the 'STM32CubeFunctionPack_MOTENV1_V3.0.0' for SensorTile platform.

I does support the USBD_cdc function in sending data to PC (Print) but missing the receive code.

Since there is a ST BLE on board, I would like to connect with the 'BlueNRG GUI' tools which I can perform firmware update through USB for ST-BLE.

1. Where I could find the example code for USBD receive for STM32L4 ?

2. Is 'BlueNRG DK 2.0.2\Projects\Projects_Cube\BlueNRG_Stack_IFR_Updater' be the right package to start ?

Thanks

    This topic has been closed for replies.

    1 reply

    ST Technical Moderator
    September 22, 2017
    Posted on September 22, 2017 at 18:57

    Hi,

    Have a look to the

    http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-embedded-software/stm32cubel4.html

    firmware package to find the USB device example.

    You have the

    https://community.st.com/0D50X00009XkffXSAR

    Bluetooth Low Energy software expansion for STM32Cube, you can start with thesample applications in Projects\Multi\Applications and followthe instructions provides in thereadme.txt file to run the example.

    Best Regards

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks