Skip to main content
JDarg
Associate II
April 25, 2019
Question

STM32L4 SPI interface to Flash Memory Winbond W25Q80DV

I am trying to interface with the Winbond W25Q80DV which is a SPI flash memory chip. I am using the STM32L476VG development board. To test the connection I am first trying to read the manufacturing ID from the chip. Using an oscilloscope I am able to see that the clock signal, chip select, and data in all look correct. The data out line is inconsistent and shows data but the data is incorrect and doesn't repeat. I have tried some other commands as well in which I am able to get a response, but again the response is incorrect and inconsistent. I have slowed my clock down, and tried some other HAL settings but in my mind they appear to be correct. Any insight or debugging advice?

For the setup, hold pin and write protect are held high.

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * <h2><center>&copy; Copyright (c) 2019 STMicroelectronics.
 * All rights reserved.</center></h2>
 *
 * This software component is licensed by ST under BSD 3-Clause license,
 * the "License"; You may not use this file except in compliance with the
 * License. You may obtain a copy of the License at:
 * opensource.org/licenses/BSD-3-Clause
 *
 ******************************************************************************
 */
/* USER CODE END Header */
 
/* Includes ------------------------------------------------------------------*/
#include "main.h"
 
SPI_HandleTypeDef hspi1;
 
 
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_SPI1_Init(void);
 
 
/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_SPI1_Init();
 /* USER CODE BEGIN 2 */
 
 uint8_t spiflash [8] = {};
 uint8_t message2[8]={};
 
 spiflash[0]=0x90;
 
 HAL_Delay(10);
 while (1)
 {
 /* USER CODE END WHILE */
	 HAL_GPIO_WritePin(GPIOE, GPIO_PIN_12, GPIO_PIN_SET);
	 HAL_GPIO_WritePin(GPIOE, GPIO_PIN_12, GPIO_PIN_RESET);
 
	 HAL_SPI_TransmitReceive(&hspi1, (uint8_t *)spiflash, (uint8_t *)message2, 8, HAL_MAX_DELAY);
	 HAL_GPIO_WritePin(GPIOE, GPIO_PIN_12, GPIO_PIN_SET);
 
	 HAL_Delay(10);
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}
 
/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
 RCC_OscInitStruct.MSIState = RCC_MSI_ON;
 RCC_OscInitStruct.MSICalibrationValue = 0;
 RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_2;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure the main internal regulator output voltage 
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
 {
 Error_Handler();
 }
}
 
/**
 * @brief SPI1 Initialization Function
 * @param None
 * @retval None
 */
static void MX_SPI1_Init(void)
{
 
 /* USER CODE BEGIN SPI1_Init 0 */
 
 /* USER CODE END SPI1_Init 0 */
 
 /* USER CODE BEGIN SPI1_Init 1 */
 
 /* USER CODE END SPI1_Init 1 */
 /* SPI1 parameter configuration*/
 hspi1.Instance = SPI1;
 hspi1.Init.Mode = SPI_MODE_MASTER;
 hspi1.Init.Direction = SPI_DIRECTION_2LINES;
 hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
 hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi1.Init.NSS = SPI_NSS_SOFT;
 hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;
 hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi1.Init.CRCPolynomial = 7;
 hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
 hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
 if (HAL_SPI_Init(&hspi1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN SPI1_Init 2 */
 
 /* USER CODE END SPI1_Init 2 */
 
}
 
/**
 * @brief GPIO Initialization Function
 * @param None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOE_CLK_ENABLE();
 
}
 
/* USER CODE BEGIN 4 */
 
/* USER CODE END 4 */
 
/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 
 /* USER CODE END Error_Handler_Debug */
}
 
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @param file: pointer to the source file name
 * @param line: assert_param error line source number
 * @retval None
 */
void assert_failed(char *file, uint32_t line)
{ 
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
void HAL_SPI_MspDeInit(SPI_HandleTypeDef* hspi)
{
 if(hspi->Instance==SPI1)
 {
 /* USER CODE BEGIN SPI1_MspDeInit 0 */
 
 /* USER CODE END SPI1_MspDeInit 0 */
 /* Peripheral clock disable */
 __HAL_RCC_SPI1_CLK_DISABLE();
 
 /**SPI1 GPIO Configuration 
 PA5 ------> SPI1_SCK
 PE12 ------> SPI1_NSS
 PE14 ------> SPI1_MISO
 PE15 ------> SPI1_MOSI 
 */
 HAL_GPIO_DeInit(GPIOA, GPIO_PIN_5);
 
 HAL_GPIO_DeInit(GPIOE, GPIO_PIN_12|GPIO_PIN_14|GPIO_PIN_15);
 
 /* USER CODE BEGIN SPI1_MspDeInit 1 */
 
 /* USER CODE END SPI1_MspDeInit 1 */
 }
 
}

This topic has been closed for replies.

4 replies

Vangelis Fortounas
Associate II
April 25, 2019

Hi.

Seems Dout pis is in float state.

Is /HOLD pin connected to vcc?

JDarg
JDargAuthor
Associate II
April 26, 2019

Thanks for the input. Yes, the hold pin is connected to VCC.

EPapa
Visitor II
May 29, 2019

@JDarg​  i’ve the same problem. How did you solve it??

JDarg
JDargAuthor
Associate II
June 2, 2019

Added a pull up resistor on MOSI and MISO and used PE13 for clock instead of PA5. On the dev board PA5 is connected to a cap that was messing up the clock signal.