Skip to main content
Gerardo GALLUCCI
ST Employee
Mar 15, 2018 6:43 PM UTC
Solved

STM32L4 RTC

Posted on March 15, 2018 at 19:43

Hi all,

I'm facing an odd behavior working with an L4/Nucleo64/CubeMX/HAL. RTC peripheral. Same result w/ and w/o LSE oscillator.

Basically, a code like this:

while (1) {

   HAL_RTC_GetTime(&hrtc, &sTime, FORMAT_BCD);

   HAL_RTC_GetDate(&hrtc, &sDate, FORMAT_BCD);

   printf('DateTime ......', ......, sTime.Hours, sTime.Minutes, sTime.Seconds);

   HAL_Delay(1000);

}

Results in:

DateTime - 1/1/2000-1-0:0:0

DateTime - 1/1/2000-1-0:0:1

DateTime - 1/1/2000-1-0:0:2

DateTime - 1/1/2000-1-0:0:3

DateTime - 1/1/2000-1-0:0:4

DateTime - 1/1/2000-1-0:0:5

DateTime - 1/1/2000-1-0:0:6

DateTime - 1/1/2000-1-0:0:7

DateTime - 1/1/2000-1-0:0:8

DateTime - 1/1/2000-1-0:0:9 

DateTime - 1/1/2000-1-0:0:16

DateTime - 1/1/2000-1-0:0:17

DateTime - 1/1/2000-1-0:0:18

DateTime - 1/1/2000-1-0:0:19

DateTime - 1/1/2000-1-0:0:20

DateTime - 1/1/2000-1-0:0:21

DateTime - 1/1/2000-1-0:0:22

DateTime - 1/1/2000-1-0:0:23

DateTime - 1/1/2000-1-0:0:24

DateTime - 1/1/2000-1-0:0:25

DateTime - 1/1/2000-1-0:0:32

...

DateTime - 1/1/2000-1-0:0:56

DateTime - 1/1/2000-1-0:0:57

DateTime - 1/1/2000-1-0:0:64

DateTime - 1/1/2000-1-0:0:65

...

DateTime - 1/1/2000-1-0:0:88

DateTime - 1/1/2000-1-0:0:89

DateTime - 1/1/2000-1-0:1:0

DateTime - 1/1/2000-1-0:1:1

So:

  • every 10 accesses to GetTime, RTC jumps 7 seconds after;
  • seconds counts up to 90. Probably minutes and hours will be wrong later.

Any idea?

    This topic has been closed for replies.
    waclawek.jan
    waclawek.janBest answer
    Super User
    Mar 15, 2018 9:41 PM UTC
    Posted on March 15, 2018 at 22:41

    BCD means Binary Coded Decimal  (more precisely it's packed BCD).

    In BCD, you count

    0x00, 0x01, 0x02... 0x09, 0x10, 0x11, 0x12... 0x58, 0x59, 0x00, 0x01...

    But you then take those BCD numbers and print them in decimal, which for the same sequence as above is:

       0,    1,    2...    9,   16,   17,   18...   88,   89,    0,    1....

    and that's exactly what you observe.

    JW

    1 reply

    waclawek.jan
    waclawek.janBest answer
    Super User
    Mar 15, 2018 9:41 PM UTC
    Posted on March 15, 2018 at 22:41

    BCD means Binary Coded Decimal  (more precisely it's packed BCD).

    In BCD, you count

    0x00, 0x01, 0x02... 0x09, 0x10, 0x11, 0x12... 0x58, 0x59, 0x00, 0x01...

    But you then take those BCD numbers and print them in decimal, which for the same sequence as above is:

       0,    1,    2...    9,   16,   17,   18...   88,   89,    0,    1....

    and that's exactly what you observe.

    JW