Skip to main content
JDarg
Associate II
July 24, 2019
Question

STM32L4 not exiting sleep mode

When trying to implement sleep mode it appears the code enters and exits sleep mode once and then gets stuck in sleep mode after and will not wake back up. I posted some code below of what I believe affects the sleep function. I want the code to sleep, wake up due to interrupt and perform function, and then go back to sleep until next interrupt. Using STM32L476VG and True Studio

void init_All(void){
	MICRO_SPI_Init();
	init_wireless();
 FLASH_INIT();
 power_init();
 enter_sleep();
}
int main(void)
{
 HAL_Init();
 
 
 /* Configure the system clock */
 
 SystemClock_Config();
 
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_SPI3_Init();
 MX_SPI2_Init();
 MX_UART4_Init();
 MX_USART1_UART_Init();
 
 __HAL_UART_ENABLE_IT(&huart4, UART_IT_RXNE);		//Enables Receive Interrupt
	init_All();
	done=1;
 while(1){
 }
 
}
 
 
static void MX_GPIO_Init(void)
{
/* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOE_CLK_ENABLE();
 
 GPIO_InitStruct.Pin = MICRO_CS;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(MICRO_CS_PORT, &GPIO_InitStruct);
 
 /* EXTI interrupt init ERB Clock Select EXTI12*/
 HAL_NVIC_SetPriority(EXTI2_IRQn, 1, 0);
 HAL_NVIC_EnableIRQ(EXTI2_IRQn);
}
 
/* USER CODE BEGIN 4 */
 
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
 
{
 
	if (GPIO_Pin==MICRO_CS)
	{
	HAL_ResumeTick();
	if (done==1){
		sendDataState();
	}
 
	 enter_sleep();
	}
 
}

void power_init(void)
 
{
 
	 /* Disable Prefetch Buffer */
 
	 __HAL_FLASH_PREFETCH_BUFFER_DISABLE();
 
 
 
	 /* Reset all RCC Sleep and Stop modes register to */
 
	 /* improve power consumption */
 
	 RCC->AHB1SMENR = 0x0;
 
	 RCC->AHB2SMENR = 0x0;
 
	 RCC->AHB3SMENR = 0x0;
 
 
 
	 RCC->APB1SMENR1 = 0x0;
 
	 RCC->APB1SMENR2 = 0x0;
 
	 RCC->APB2SMENR = 0x0;
 
 
 
	 /* Configure the system Power */
 
	 SystemPower_Config();
 
}
 
/**
 
 * @brief System Power Configuration
 
 * @retval None
 
 */
 
void SystemPower_Config(void)
 
{
 
 GPIO_InitTypeDef GPIO_InitStructure;
 
 
 
 /* Set all GPIO in analog state to reduce power consumption */
 
 __HAL_RCC_GPIOA_CLK_ENABLE();
 
 __HAL_RCC_GPIOB_CLK_ENABLE();
 
 __HAL_RCC_GPIOC_CLK_ENABLE();
 
 __HAL_RCC_GPIOD_CLK_ENABLE();
 
 __HAL_RCC_GPIOE_CLK_ENABLE();
 
 __HAL_RCC_GPIOF_CLK_ENABLE();
 
 __HAL_RCC_GPIOG_CLK_ENABLE();
 
 __HAL_RCC_GPIOH_CLK_ENABLE();
 
 
 
 GPIO_InitStructure.Mode = GPIO_MODE_ANALOG;
 
 GPIO_InitStructure.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 
 GPIO_InitStructure.Pull = GPIO_NOPULL;
 
 GPIO_InitStructure.Pin = GPIO_PIN_All;
 
 
 
 HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
 
 HAL_GPIO_Init(GPIOB, &GPIO_InitStructure);
 
 HAL_GPIO_Init(GPIOC, &GPIO_InitStructure);
 
 HAL_GPIO_Init(GPIOD, &GPIO_InitStructure);
 
 HAL_GPIO_Init(GPIOE, &GPIO_InitStructure);
 
 HAL_GPIO_Init(GPIOF, &GPIO_InitStructure);
 
 HAL_GPIO_Init(GPIOG, &GPIO_InitStructure);
 
 HAL_GPIO_Init(GPIOH, &GPIO_InitStructure);
 
 
 
 __HAL_RCC_GPIOA_CLK_DISABLE();
 
 __HAL_RCC_GPIOB_CLK_DISABLE();
 
 __HAL_RCC_GPIOC_CLK_DISABLE();
 
 __HAL_RCC_GPIOD_CLK_DISABLE();
 
 __HAL_RCC_GPIOE_CLK_DISABLE();
 
 __HAL_RCC_GPIOF_CLK_DISABLE();
 
 __HAL_RCC_GPIOG_CLK_DISABLE();
 
 __HAL_RCC_GPIOH_CLK_DISABLE();
 
 
 
 /* Enable PWR clock */
 
 __HAL_RCC_PWR_CLK_ENABLE();
 
 
 
 
 
 //Under Voltage Protection
 
 PWR_PVDTypeDef sConfigPVD = { 0 };
 
 
 
 //2.9 V under voltage
 
 sConfigPVD.PVDLevel =PWR_PVDLEVEL_6;
 
 HAL_PWR_ConfigPVD(&sConfigPVD);
 
 HAL_PWR_EnablePVD();
 
 HAL_NVIC_SetPriority(PVD_PVM_IRQn, 0, 0);
 
 HAL_NVIC_EnableIRQ(PVD_PVM_IRQn);
 
 
 
}
 
 
 
/**
 
 * @brief Enter Sleep Mode
 
 * @retval None
 
 */
 
void enter_sleep(void){
 
 
 
 /*Suspend Tick increment to prevent wakeup by Systick interrupt.
 
 Otherwise the Systick interrupt will wake up the device within 1ms (HAL time base)*/
 
 HAL_SuspendTick();
 
 
 
	 /* Enter Sleep Mode , wake up is done once User push-button is pressed */
 
	 HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);
 
 
 
}

This topic has been closed for replies.