STM32L4.. fs=10Ksps ADC Current, how do you get the stated 16uA?
In the data sheet it states that the ADC current at fs=10Ksps is 16 microAmps. I'm struggling to get the current that low. Even just switching on the ADC and its regulator exceeds that value
My application has a mode where I need the ADC data passed through to the DAC (unchanged) with the lowest current possible (coin cell application). Sample rate is 16,384Hz derived from TMR2 (with LSE=32,768Hz). I trigger the ADC with TMR2 and DMA the result straight to the DAC. The system clock is MSI=1 MHz , with the CPU in LPSLEEP.
Anyway, since this 10Ksps= 16uA is stated in the data sheet, I thought maybe the ST engineers could state how this current consumption could be achieved,
thanks