STM32L4 - are pullups during reset active when RDP level is 2?
Citing from the STM32L431 manual:
The debug pins are in AF pull-up/pull-down after reset:
• PA15: JTDI in pull-up
• PA14: JTCK/SWCLK in pull-down
• PA13: JTMS/SWDAT in pull-up
• PB4: NJTRST in pull-up
• PB3: JTDO in floating state no pull-up/pull-down
Let's take PA15 as an example. What happens if RDP level is set to level 2 (debug interface disabled). Will the debug pin pulls still be active?