Skip to main content
Miha Mohor?i?
Associate
Oct 11, 2017 10:26 AM UTC
Solved

Stm32l4 1.9.0 - FatFs naming problem

Posted on October 11, 2017 at 12:26

Hi, 

I am using package Stm32l4 1.9.0 package on Linux with Stm32CubeMX to generate workbench project. 

It seems there is naming problem, since folder in downloaded repository is named 

'STM32Cube_FW_L4_V1.9.0/Middlewares/Third_Party/FatFS'

while it should be 

'STM32Cube_FW_L4_V1.9.0/Middlewares/Third_Party/FatFs'

This causes problem during build and code generation. Repository was updated using CubeMX. 

Can somebody replicate this, or is something wrong with my configuration? 

I hope i am not duplicating this issue. 

Best Regards, Miha 

    This topic has been closed for replies.
    Tilen MAJERLE
    Tilen MAJERLEBest answer
    ST Employee
    Oct 11, 2017 12:01 PM UTC
    Posted on October 11, 2017 at 14:01

    Hello

    Mohor_i_.Miha

    ‌,

    I can confirm a problem with this package. Currently, please manually correct the mistake.

    Best regards,

    Tilen

    4 replies

    AvaTar
    Senior III
    Oct 11, 2017 11:51 AM UTC
    Posted on October 11, 2017 at 13:51

    Can somebody replicate this, or is something wrong with my configuration? 

    I leave that for ST, but it is quite probable they never ever tried with a case-sensitive file system.

    Tilen MAJERLE
    Tilen MAJERLEBest answer
    ST Employee
    Oct 11, 2017 12:01 PM UTC
    Posted on October 11, 2017 at 14:01

    Hello

    Mohor_i_.Miha

    ‌,

    I can confirm a problem with this package. Currently, please manually correct the mistake.

    Best regards,

    Tilen

    Kevin Goez
    Visitor II
    Oct 11, 2017 12:07 PM UTC
    Posted on October 11, 2017 at 14:07

    Hello, I can confirm this issue. I just logged in to post the same problem.

    The 1.9.0 firmware contains the wrong capitilization 'FatFS'. Generation fails. Changing this manually to 'FatFs' seems to fix the issue.

    Problem occurs in Linux, where case matters...

    In STM32Cube_FW_L4_V1.8.0, the directory was correct with 'FatFs' and worked fine.

    It would be helpful if the CubeMx debug output would spit out an error that helped the user find the problem. Took me a while to locate the root cause why FatFs wasnt being generated.

    Amel NASRI
    ST Technical Moderator
    Oct 13, 2017 11:41 AM UTC
    Posted on October 13, 2017 at 13:41

    Hi,

    I would like to inform you the folder '

    Middlewares/Third_Party/FatFS' will be renamed '

    Middlewares/Third_Party/FatFs' in the coming release of the STM32CubeL4 package (V1.10.0) which is expected to be available by the end of October.

    Sorry for any inconvenience this created for you.

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.