Skip to main content
moran
Associate III
May 3, 2015
Question

STM32L152 Wrong ADC values

  • May 3, 2015
  • 1 reply
  • 664 views
Posted on May 03, 2015 at 16:46

Hello,

I'm working on custom board using STM32L152 chip.

Vref is : 3.19V

When i injuct to the analog pin 2.7 i read 4019 ,while 0 represent as 650.

(It seemed like 650 is the gap ????)

below my initialize ADC code :

/////////////////////////////////////////////

RCC_HSICmd(ENABLE);

 RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);

  

 // Configuration CURRENT_SNS pins

 //~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

        a_opAdcControl->m_oAdcGpioControl.GPIO_Pin = GPIO_Pin_1;

        a_opAdcControl->m_oAdcGpioControl.GPIO_Mode = GPIO_Mode_AN;

        GPIO_Init(GPIOC, &a_opAdcControl->m_oAdcGpioControl);

       

  

 // Configuration Battary test

 //~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

// RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);

  

// a_opAdcControl->m_oAdcGpioControl.GPIO_Pin = GPIO_Pin_4;

// a_opAdcControl->m_oAdcGpioControl.GPIO_Mode = GPIO_Mode_AN;

// GPIO_Init(GPIOA, &a_opAdcControl->m_oAdcGpioControl);

  

   // Check that HSI oscillator is ready

   while(RCC_GetFlagStatus(RCC_FLAG_HSIRDY) == RESET);

 // ADC1 Configuration ------------------------------------------------------

 RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);

 // ADC1 DeInit

 ADC_DeInit(ADC1);

  

 // ADC1 Configuration

 a_opAdcControl->m_oAdcInitControl.ADC_Resolution = ADC_Resolution_12b;

 a_opAdcControl->m_oAdcInitControl.ADC_ScanConvMode = DISABLE;// Disable multichannels

 a_opAdcControl->m_oAdcInitControl.ADC_ContinuousConvMode = DISABLE;// One Conversion at a time

 a_opAdcControl->m_oAdcInitControl.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;//ADC_ExternalTrigConvEdge_Rising;//ADC_ExternalTrigConvEdge_Falling;

 a_opAdcControl->m_oAdcInitControl.ADC_ExternalTrigConv =0;

 a_opAdcControl->m_oAdcInitControl.ADC_DataAlign = ADC_DataAlign_Right;

 a_opAdcControl->m_oAdcInitControl.ADC_NbrOfConversion = 1;

 ADC_Init(ADC1, &a_opAdcControl->m_oAdcInitControl);

  

 // ADC1 Regular Channel Config

  

   

 // Enables the ADC1 Power Down during Delay

 ADC_PowerDownCmd(ADC1, ADC_PowerDown_Idle_Delay, ENABLE);

  

 // Delay until the converted data has been read

 ADC_DelaySelectionConfig(ADC1, ADC_DelayLength_Freeze);

 // Enable ADC1

 ADC_Cmd(ADC1, ENABLE);    

 

 // Wait until the ADC1 is ready

 while(ADC_GetFlagStatus(ADC1, ADC_FLAG_ADONS) == RESET)

 {

 }

////////////////////////////////////////////////////////////////

The code for reading ch :

// a_selCH = 0x0B (ch11 --> PC-1)

ADC_RegularChannelConfig(ADC1, a_selCH, 1, ADC_SampleTime_4Cycles);

  ADC_ClearFlag(ADC1,ADC_FLAG_EOC);

  // Start the conversion

  ADC_SoftwareStartConv(ADC1);

  // Wait until conversion completion

  while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET){}

  // Get the conversion value

  if (ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == SET)

  {

    g_opAdcControl->m_oAdcChSample = ADC_GetConversionValue(ADC1);

  }

  ADC_ClearFlag(ADC1, ADC_FLAG_EOC);

////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

 

Please advise,

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    May 3, 2015
    Posted on May 03, 2015 at 17:44

    Try it with more that 4 cycles, and on an STM32L1-DISCO or NUCLEO board.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..