Skip to main content
TPati.2
Visitor II
Mar 10, 2021 1:44 PM UTC
Solved

STM32L152-DISCOVERY Touch Sensing.Can i know the procedure or sample code for enabling Touch Sensing to control led as i am not able to get any detailed information for the same from the online tutorial or pdf .I need to know it urgently.

Just need to know if i have to enable the touch sensing through code or manually and need to the process for the same.Thanks.

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Mar 15, 2021 9:29 AM UTC

Hello @TPati.2​ and welcome to the STM32 Community =)

I recommended you to start from the TouchSensing application under the STM32CubeL1 MCU package:

\STM32Cube_FW_L1_V1.10.2\Projects\STM32L152D-EVAL\Applications\TouchSensing

You may find clarification and more details on how to use the TSL referring to the following resources:

  • AN5105 "Getting started with touch sensing control on STM32 microcontrollers", which helps you on how to set-up an TSC application using STM32CubeMX applicable for several TSC series such as STM32L1, F3, L0, and L4.
  • UM1913 Developing applications on STM32Cube with touch sensing
  • Several TSC related resources are available on the ST web site. Ex: AN3236, AN3960,AN4310, AN4313, AN4312,...

I hope this resources are helpful for you.

Please mark my answer as "Best Answer" by clicking on the "Select as Best" button if it helped :smiling_face_with_smiling_eyes:.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

1 reply

Imen.DBest answer
ST Technical Moderator
Mar 15, 2021 9:29 AM UTC

Hello @TPati.2​ and welcome to the STM32 Community =)

I recommended you to start from the TouchSensing application under the STM32CubeL1 MCU package:

\STM32Cube_FW_L1_V1.10.2\Projects\STM32L152D-EVAL\Applications\TouchSensing

You may find clarification and more details on how to use the TSL referring to the following resources:

  • AN5105 "Getting started with touch sensing control on STM32 microcontrollers", which helps you on how to set-up an TSC application using STM32CubeMX applicable for several TSC series such as STM32L1, F3, L0, and L4.
  • UM1913 Developing applications on STM32Cube with touch sensing
  • Several TSC related resources are available on the ST web site. Ex: AN3236, AN3960,AN4310, AN4313, AN4312,...

I hope this resources are helpful for you.

Please mark my answer as "Best Answer" by clicking on the "Select as Best" button if it helped :smiling_face_with_smiling_eyes:.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks