Question
STM32L152: Connect the COMP2 output to the IO port
Posted on June 01, 2018 at 11:22
I want to connect the COMP2 output to the external circuit.
I know the output can be redirected to the IC channel of some timers.
and I tried to use TIM2_IC4 to get the output of COMP2 but failed.
Is it possible to implement in STM32L152C8?
Because it is a low-power application, I do not want to use interrupt to achieve this.