Skip to main content
Jyoun.1
Visitor II
March 22, 2021
Question

STM32L151CBU6 Firmware Download problem

  • March 22, 2021
  • 1 reply
  • 791 views

Hi, everyone

I, Currently STM32L151CBU6 is in use.

The firmware uses a .HEX file,

I am using the firmware download to change the boot mode.

Now, firmware download through STM FlashLoader Demo.exe(2.8.0) works normally.

However, STMFlashLoader.exe is used through the following options:

-----------------------------------------------------------------------------------------------

"STMFlashLoader.exe" -c --pn 3 --br 115200 --db 8 --pr EVEN --sb 1 --ec OFF --to 2000 --co ON 

-i STM32L1_Cat1-32K -d --o --a 8000000 --v --fn D:\CubeMX_20210317.hex

-----------------------------------------------------------------------------------------------

The download itself is returned as normal, but as a result of checking through the source

Actual download does not proceed.

Ask if it's a problem with the board or if there are other options.

--------------------------------------------------------------------------------------

 DOWNLOADING ...

 downloading   page/sector 0  @0x 8000000  size 0.25(KB)  [OK]

 downloading   page/sector 1  @0x 8000100  size 0.25(KB)  [OK]

 downloading   page/sector 2  @0x 8000200  size 0.25(KB)  [OK]

 ....

 -----------------------------------------------------------------------------------------

This topic has been closed for replies.

1 reply

ST Technical Moderator
March 30, 2021

Hello @Jyoun.1​ and welcome to the STM32 Community,

Do you have still this problem to solve?

I would advise you to try STM32Cubeprogrammer software (an all-in-one multi-OS software tool for programming STM32 products).

Please, keep us informed about your progress on this issue.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks