Skip to main content
Visitor II
November 20, 2025
Solved

stm32l151c8t6a device marking with QR code

Hi, I bought 50pcs STM32L151C8T6A from one Chinese online vendor, which has device marking with QR code.

I encountered an issue while using the new version chip, after initial power-on, the overall sleep current of the product is approximately 5uA(STM32L151C8T6A in stop mode), When I reset the product's hardware multiple times, there is a high probability that the product's sleep current will reach up to 1.6mA. Once this occurs, the product can only return to normal by being powered on again.

With the same hardware, replacing the STM32L151C8T6A with an older version will prevent the issue from occurring.

This is a mature product, and this is also my first time using the new version of STM32L151C8T6A. Is the software for the old and new versions incompatible? What should I be aware of?

ps: I am using the STM32L series standard library.

 

 

owen_chen_0-1763653398218.png

 

owen_chen_1-1763653463367.png

 

 

 

 

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
November 21, 2025

Hello @owen_chen and welcome to the ST community,

I recommend to contact your local ST sales/FAE for that.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
November 21, 2025

Hello @owen_chen and welcome to the ST community,

I recommend to contact your local ST sales/FAE for that.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.