Skip to main content
Visitor II
Mar 11, 2024 3:35 PM UTC
Solved

STM32L151 ADC

I am working with the above device. I have created an .IOC file and auto-generated code. I can see the GPIO configuration for the simple I/O, but I do not see any pin configuration for the ADC inputs that I have selected. I assume that I will have to add these to the MX_ADC_Init module.

I have attached the .IOC file that I have created.

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 11, 2024 3:51 PM UTC

Hello,

They are generated in stm32l1xx_hal_msp.c file in HAL_ADC_MspInit():

 

 /**ADC GPIO Configuration
 PF6 ------> ADC_IN27
 PF7 ------> ADC_IN28
 PC1 ------> ADC_IN11
 PC2 ------> ADC_IN12
 PC3 ------> ADC_IN13
 PA0-WKUP1 ------> ADC_IN0
 PA1 ------> ADC_IN1
 */
 GPIO_InitStruct.Pin = VCC_12V_Pin|VCC_3V3_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);

 GPIO_InitStruct.Pin = TEMPERATURE_Pin|TEMPA_Pin|TEMPB_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 GPIO_InitStruct.Pin = ISENSE_3V3_Pin|ISENSE_12V_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 

Note that HAL_ADC_MspInit() is called by HAL_ADC_Init() which in turn called by MX_ADC_Init()

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 11, 2024 3:51 PM UTC

Hello,

They are generated in stm32l1xx_hal_msp.c file in HAL_ADC_MspInit():

 

 /**ADC GPIO Configuration
 PF6 ------> ADC_IN27
 PF7 ------> ADC_IN28
 PC1 ------> ADC_IN11
 PC2 ------> ADC_IN12
 PC3 ------> ADC_IN13
 PA0-WKUP1 ------> ADC_IN0
 PA1 ------> ADC_IN1
 */
 GPIO_InitStruct.Pin = VCC_12V_Pin|VCC_3V3_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);

 GPIO_InitStruct.Pin = TEMPERATURE_Pin|TEMPA_Pin|TEMPB_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 GPIO_InitStruct.Pin = ISENSE_3V3_Pin|ISENSE_12V_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 

Note that HAL_ADC_MspInit() is called by HAL_ADC_Init() which in turn called by MX_ADC_Init()

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.